Freescale Semiconductor
G.723.1A Example Application for 5685x
Overview
The G.723.1A Demo demonstrates use of the G.723.1A library provided by the Processor Expert.
In this demo, audio is input from a PC to the G.723.1A Speech Codec (encoder and decoder) algorithm and
the decoded output is played by the G.723.1A Speech Codec on a speaker system.
How to get this software
This example application is included as part of the CodeWarrior Development Studio for 56800/E Digital
Signal Controllers. Follow these steps:
1. Install CodeWarrior Development Studio for 56800/E Digital Signal Controllers
2. Launch CodeWarrior, and create new Processor Expert project
a. Select File > New menu
b. Select Processor Expert Examples Stationery
c. Type project name
d. Click OK
e. Select DemoApplications > Telephony > G723 > 56858
f. Click OK
3. Generate application code by selecting Processor Expert > Generate Code menu
Detailed documentation
Documentation for this application is included as part of this example project. Expand Doc folder located
in the project window by clicking on the + icon next to the folder, and open desired file by double clicking it.
Freescale™ and the Freescale logo are trademarks of Freescale Semiconductor, Inc. All other product
or service names are the property of their respective owners. 
©2005, Freescale Semiconductor, Inc