Freescale Semiconductor
G.711 Example Application for 5685x
Overview
The G.711 Demo demonstrates the use of the G.711 library provided by the Processor Expert.
How to get this software
This example application is included as part of the CodeWarrior Development Studio for 56800/E Digital
Signal Controllers. Follow these steps:
1. Install CodeWarrior Development Studio for 56800/E Digital Signal Controllers
2. Launch CodeWarrior, and create new Processor Expert project
a. Select File > New menu
b. Select Processor Expert Examples Stationery
c. Type project name
d. Click OK
e. Select DemoApplications > Telephony > G711 > 56858
f. Click OK
3. Generate application code by selecting Processor Expert > Generate Code menu
Detailed documentation
Documentation for this application is included as part of this example project. Expand Doc folder located
in the project window by clicking on the + icon next to the folder, and open desired file by double clicking it.
Freescale™ and the Freescale logo are trademarks of Freescale Semiconductor, Inc. All other product
or service names are the property of their respective owners. 
©2005, Freescale Semiconductor, Inc