File: README.TPU Created by: Richard Soja, Motorola, Austin, TX 78735 Date: Jan 11, 1994 The following is a descriptive list of new public domain files which provide support for the creation of standard and new TPU functions which can be executed in emulation mode on certain 68HC16 and 683XX versions of Motorola MCUs. Please note that the .ZIP files should be de-archived in separate directories, as they each contain duplicate file names with different contents. PKZIP version 2.04 was used to archive the files. Filename Size Description -------- ---- ----------- TPUMASM EXE 128048 Version 3.33 of freeware TPU microcode assembler. This version assembles the source files found in the archive files TPUMSKA.ZIP, TPUMSKG.ZIP, TPUMISC.ZIP Please note that the source files have a completely new syntax. README CNV 7303 This text file explains all the changes in syntax for TPUMASM V3.33, and describes how to use the automated conversion program TPUCNV.EXE to convert any 'old' syntax files that you might want to re-assemble with TPUMASM.EXE TPUCNV EXE 23536 Version 0.5 of the freeware TPU source code conversion program. Converts 'old' TPU syntax to that supported by TPUMASM.EXE. Note that this program is NOT needed for the files in TPUMSKA.ZIP, TPUMSKG.ZIP, TPUMISC.ZIP as they have already been converted using this program. TPUMSKA ZIP 40751 Archive of latest microcode source files for TPU mask A functions. Use PKUNZIP version 2, or UNZIP version 5 to de-archive these files. Use TPUMASM to assemble the functions. TPUMSKG ZIP 50672 Archive of latest microcode source files for TPU mask G functions. Use PKUNZIP version 2, or UNZIP version 5 to de-archive these files. Use TPUMASM to assemble the functions. TPUMISC ZIP 42106 Archive of latest microcode source files for miscellaneous TPU functions. Use PKUNZIP version 2, or UNZIP version 5 to de-archive these files. Use TPUMASM to assemble the functions.